(0)| 3/25/2022 12:52 PM | |
|
Posts: 5 Rating:
|
Hello, I'm wondering if there is an option in TIA-portal with Startdrive V17 to use a SINAMICS S120 motor module as DC-DC converter in conjunction with batteries. As I read: SINAMICS S120 - Motor Modules als DC-DC-Converter in Kombination mit Batterien - ID: 109751796 - Industry Support Siemens this is only possible using STARTER. This is due to the technology extension ABC_OA, which I'm unable to find for Startdrive V17. Thus I'm unable to use the parameters necessary to configure the motor module as a DC-DC converter. In short: -Is it possible to set a SINAMICS S120 motor module as DC-DC converter in conjunction with batteries using Startdrive V17 Advanced? Thank you!
|
Last edited by: Groj7 at: 03/25/2022 12:54:57Last edited by: Jen_Moderator at: 03/28/2022 13:39:02Link optimized. |
|
| 3/28/2022 10:41 AM | |
|
Posts: 5 Rating:
|
Thanks for the help! |
Follow us on