6/15/2022 10:06 AM | |
Joined: 8/24/2016 Last visit: 4/22/2025 Posts: 18 Rating:
|
Hi i want the full descreption for Siemens motor part number, to be able to select a motor. if there is a website or a small program for this, kindly advice. thanks,
------------------------------------------------------------------------------------------ |
Last edited by: CS Moderator at: 06/16/2022 19:45:31New subject after splitting |
|
6/15/2022 1:02 PM | |
Joined: 4/23/2010 Last visit: 11/23/2024 Posts: 8092 Rating:
|
Please visit this page for LV motors & visit Industry Mall - Configuration Wizard wherein under Product selection/Configuration wizard you can select appropriate type of motors. Hope this helps. |
6/16/2022 2:34 PM | |
Joined: 8/24/2016 Last visit: 4/22/2025 Posts: 18 Rating:
|
Thanks for your support, but need your support to get full description for the following part number:- 1LE1543-2DB09-0AF4-Z B02+L51+M1Y+Y82 thanks in advice
|
6/17/2022 6:27 AM | |
Joined: 4/23/2010 Last visit: 11/23/2024 Posts: 8092 Rating:
|
Hello Mostafa_IPI, It is SIMOTICS standard motor self or forced air cooled cast iron motor. Frame size is 280S, without flange IM B3 construction type, terminal box at TOP. Protection - 1 KTY84 - 130 temp sensor ( 2 terminals) Please refer motor nameplate details for technical specifications since it is non standard voltage or frequency. Option B02 - Acceptance test certificate 3.1 as per EN 10204 L51 - Bearing insulation NDE M1Y - Non standard voltage or frequency. Y82 - Additional rating plate with customer specification. HTH |
Last edited by: PISCEAN 2010 at: 06/17/2022 06:44:18L51 corrected |
|
This contribution was helpful to
1 thankful Users |
Follow us on