(0)| 7/18/2022 2:20 PM | |
|
Joined: 3/5/2021 Last visit: 2/20/2025 Posts: 4 Rating:
|
Hi Denilson Thanks for your great tips on creating faceplates. I have created faceplates (symbols) from which further faceplates (details-popup) are called. From the details-popup variables can be set directly in the PLC with push buttons. This works wonderfully, because the interfaces each contain the same UDT. Now to my problem: I don't want to write the variables directly with the push buttons in the detail-popup, but call another "confirm popup". (ok/cancel) This "Confirm-Popup" should of course be universal, that means for different Push Buttons/Variables in the same UDT and for different UDTs. However, I don't understand how to pass the data. In the "confirm popup" I would simply define a boolean variable in the interface, but how can I link this variable from the call? Creating a separate "Confirm-Popup" for each faceplate type and the push buttons it contains can't be the solution after all.... I would be very happy if you could give me a solution/hint to my problem. thank you very much ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 07/19/2022 07:28:58New subject after splitting |
|
Follow us on