(0)| 10/12/2022 12:30 PM | |
|
Joined: 1/31/2022 Last visit: 12/1/2025 Posts: 5 Rating:
|
Hi all! We have S7-1500 PLC and ABB UMC100.3 relay.Both are communicating over proffibus. Apart from the data we are receiving over proffibus from the device there is a seperate wizard is being opened from the GSD file called 'Device-specific parameters'.Every parameter of the device can be accessed as well as changed from this wizard.Screenshot for the same is attached. Need help regarding how this parameters can be accessed via program (TIA portal V16) or can we generate direct tags out of this wizard? Thanks ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 10/13/2022 07:17:34New subject after splitting |
|
Follow us on