(0)| 5/28/2022 12:05 PM | |
|
Posts: 2 Rating:
|
Hello everyone; İm trying to integrate ABB relay REU615C and REF615C with SICAM PAS, i did all the IEC61850 settings and upload the SCD file into SICAM PAS and the same file also uploaded to relay but i still get the message on SICAM PAS OPERATION that says (object directory mismatched check your ICD/SCD file), inside PCM600 V2.10 there is a write option that i use to upload the configuration to device, but there is also another one which is upload to IED but this one is only from the front port and it might be for firmware upgrade which im not planning on doing, if anybody can help that would be very appreciated, Best regards; Saad BOUADI ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 05/30/2022 10:38:34New subject after splitting |
|
| 12/22/2022 2:09 PM | |
|
Joined: 6/3/2021 Last visit: 3/19/2025 Posts: 2 Rating:
|
Hi, have you tried to save the cid file using IED scout app? |
Follow us on