(0)| 2/8/2023 3:28 PM | |
|
Joined: 4/28/2018 Last visit: 12/2/2024 Posts: 3 Rating:
|
Hello, I want help for generating text List and Graphic List in WinCC Unified V18 with the help of SivArc. I have referred following help , but I am not understanding where to use following expression SetGraphicList("G_List_1") SetTextList("G_List_1") Pls refer to the attached file. For Unified devices: 1. You can configure GraphicList through Resource List available under SiVARc properties. The expression SetGraphicList("G_List_1") is used to set the Graphic List property. 2 You can configure TextList through Resource List available under SiVARc properties. The expression SetTextList("G_List_1") is used to set the Text List property. Note To configure Graphic lists for “Resource list” property, its mandatory to use “Set- GraphicList” expression. Else, system treats it as text list and accordingly messages ------------------------------------------------------------------------------------------ AttachmentExample_Creating generation templates for text lists.pdf (585 Downloads) |
Last edited by: Jen_Moderator at: 02/09/2023 10:19:10New subject after splitting |
|
Follow us on