(0)| 4/1/2023 11:00 AM | |
|
Posts: 2 Rating:
|
Hello, did you find answer to your issue ,also my self i have almost the same pb , i need that the unit to run in auto with analog input from an another source ,namenly on 0V to have 15Hz and to 10 to have 50Hz ,if you can give me some hints it will be helpful. Manny thanks! ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 04/03/2023 11:06:05New subject after splitting |
|
| 4/3/2023 11:07 AM | |
|
Posts: 8171 Rating:
|
Closed cause question posted twice. The second thread with the subject unable to set G120x in auto mode with analog input. is published within the conference SINAMICS G. Jen_Moderator |
Follow us on