(0)| 4/14/2023 8:00 PM | |
|
Joined: 10/22/2020 Last visit: 10/1/2024 Posts: 169 Rating:
|
Hello there, have a look at NodeRED. The program is already pre-installed in the example image of the IOT and starts automatically. You can access the programming interface via the IP address of the IOT on port 1880 in a browser (for example 192.168.0.1:1880). Some modules are also pre-installed and you should have a look at this MindConnect module. Depending on the overall information flow at the customer, other modules (S7, OPCUA, ... ) can be helpful. BR |
Follow us on