(0)| 4/25/2023 12:47 PM | |
|
Joined: 1/21/2013 Last visit: 12/24/2025 Posts: 4365 Rating:
|
Hi Peter, Unfortunately, I can only answer some of your questions. All Windows CE based devices only support SMB 1.0 and there are no plans to change this. Instead of using the outdated SMB 1.0 protocol, Siemens recommends using the HMI Option+ Manager. Unified Comfort Panels require SMB 3.0 to connect a network drive. Unfortunately, I can't provide much information on the requested topics WINS and SIMATIC Logon. However, there is a FAQ which states that SIMATIC Logon can be used with a fixed IP address instead of a domain name. For UMC I couldn't find any information about WINS, so I assume that it is not used there. Kind regards |
This contribution was helpful to
|
|
Follow us on