(0)| 5/25/2023 5:03 PM | |
|
Posts: 3 Rating:
|
Hello, I have issue with analog bar - cannot retentive value from the bar. After power on value is 0. On the animation settings this bar can be 15 minimum and 24 maximum. Blok type VW. When I set this bar once the only value with can be is from 15 to 24 (what is ok ) but after logo start and i do not touch bar the value is 0. Any ideas ? Regards Peter AttachmentAnalog bar.zip (635 Downloads) |
| 5/26/2023 3:50 PM | |
|
Joined: 12/18/2014 Last visit: 1/14/2026 Posts: 36457 Rating:
|
The same ask you in this topic: Analog bar retentive for power failure or stop modePlease don't post twice for the same problem. |
This contribution was helpful to
|
|
| 5/30/2023 8:12 AM | |
|
Posts: 8171 Rating:
|
Closed cause question posted twice. The second thread with the subject Analog bar retentive for power failure or stop mode is published within the conference LOGO! - Software. Best regards, |
Follow us on