(1)| 7/20/2023 7:02 AM | |
|
Posts: 7 Rating:
|
Dear all, I have a problem with the external SSI encoder that is main synchronous axis (leading value) for the two following axes. The problem is that the actual velocity jumps very high for a moment (~1ms) from a value of 240 deg/sek to --359758deg/sec always in the same position. I have no problem with the actual position. This big negative velocity value changes the extrapolated position and velocity as shown in the pictures. I tried using velocity filters without success. I cannot use tolerance band width because of the high difference in actual velocity. Have anyone faced the same problem? Best regards AttachmentDownloads.zip (382 Downloads) |
| 7/20/2023 8:56 AM | |
|
Posts: 158 Rating:
|
Hello Kokabt, we need more information to be able to help you: Template for the new topics |
Follow us on