(0)| 8/8/2023 1:50 PM | |
|
Joined: 1/24/2022 Last visit: 6/5/2024 Posts: 1 Rating:
|
Hello, I would like to ask what is the meaning of the below values in 6ES7132-4BF00-0AA0 DO. Output current ● for signal "1" rated value 0.5 A ● for signal "1" permissible range, min. 7 mA ● for signal "1" permissible range, max. 600 mA ● for signal "0" residual current, max. 0.3 mA I would like to ask what do i consider to calculate the consumption on this card. Other values given are as below: Input current from load voltage L+ (without load), max. 5 mA; Per channel from backplane bus 3.3 V DC, max. 10 mA ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 08/09/2023 08:17:41New subject after splitting |
|
Follow us on