(0)| 8/21/2023 7:23 PM | |
|
Joined: 6/4/2008 Last visit: 11/25/2025 Posts: 1521 Rating:
|
Hi Tony, Various options for You, depending on "how damaged" the Micromaster is, you could attempt to upload the parameters into an Advanced Operator Panel and then download into your new one. Failing that, You could attempt to download the original file just using Drivemonitor, but I've had varied success, especially with the later firmwares in the Micromasters. The recommended method today is to use the Starter software, downloadable from here: Sinamics (and Micromaster) Starter If you wish to use it, download the three zip files presented for version 5.5 HF1 and MAKE SURE you read and follow the "Installation procedure for STARTER V5.5 HF1" as this is one of the most common reasons for the software not working. Using the script in the FAQ listed below, it is possible to convert the DNL file to a format suitable for Starter (Personally I would just recommission it in Starter, but that's just my choice) Drivemonitor .DNL to Starter conversion script FAQ I assume that you have hardware (i.e. cable) in order to connect to the MM4. PC-MM4 connection kit - 6SE6400-1PC00-0AA0 MM4 AOP - 6SE6400-0AP00-0AA1 Please note these are now both classed as spare parts and are charged accordingly on the second hand markets. Regards, Graeme |
This contribution was helpful to
|
|
Follow us on