(1)| 6/24/2009 11:55 AM | |
|
Posts: 45 Rating:
|
Hello everybody. Recently installed PLCSIM V5.4 SP3 with a hope to try multiprocessor simulation. As declared by SIEMENS in S7-PLCSIM V5.4 SP3 Released for Delivery , "Multiple startability (multi-instance capability) and communication support between the simulated CPUs (simulation instance)" is supported in this version Several instances can be started simultaneously all right, each having its window name S7-PLCSIM1, S7-PLCSIM2, etc. BUT!!! External applications may communicate via COM-object S7ProSim only with a first instance named S7-PLCSIM1 ! Moreover, as far as i'm concerned, there are no settings inS7ProSim to specify wich instance you want to access Can anybody tell is this a bug or featue? |
Last edited by: SSE at: 6/24/2009 12:27 PM |
|
| 6/24/2009 1:36 PM | |
|
Posts: 34 Rating:
|
Use the ConnectExt method. Doesn't seem to be in the documentation, it is available however. |
This contribution was helpful to
|
|
| 6/24/2009 1:53 PM | |
|
Posts: 45 Rating:
|
Thanks a lot! The question is solved |
Follow us on