(0)| 8/11/2024 3:06 PM | |
|
Joined: 11/21/2020 Last visit: 8/26/2025 Posts: 213 Rating:
|
I'm using 1215 PLC. Program is attached, so you can check it yourself. I want pretend that I'm familiar with subject, it is my first program of this kind. AttachmentStepper Control 1215 CPU.zip (401 Downloads) |
| 8/12/2024 6:59 AM | |
|
Joined: 11/21/2020 Last visit: 8/26/2025 Posts: 213 Rating:
|
I am using Stepper Online's CLT57T V4.1 stepper drive ( https://www.omc-stepperonline.com/en-au/closed-loop-stepper-driver-v4-1-0-8-0a-24-48vdc-for-nema-17-23-24-stepper-motor-cl57t-v41 ) with 23HS45-4204D-E1000 stepper motor ( https://www.omc-stepperonline.com/en-au/nema-23-closed-loop-stepper-motor-3-0nm-424oz-in-encoder-1000ppr-4000cpr-23hs45-4204d-e1000 ) and 1215C PLC + TP700. For now there is no control strategy, I am just getting familiar with motor control. I used as base for my program an example that I found on youtube. Commands I'm testing manually using TP700. The only way to increase max velocity is to decrease mechanics/Pulses per motor revolution below 6400 (with 6400 setting stepper runs only if max velocity is below 1400 degree/s or 781 mm/s). CLT57T is set to 6400 pulses/rev, motor runs only if max velocity is less than 1400 degrees/s. CTL supports up to 51200 pul/rev, does it change anything? I have noticed that in TIA axis configuration velocity could be boosted only if Mechanics/Pulses per motor revolution setting is decreased. Is it possible/of any use to connect stepper's encoder to PLC? I suppose that it is TTL encoder since it is powered with 5V DC? I have TTL to HTL encoder converter, I guess it could be used instead of S7-1200 module for TTL encoders. I saw that encoder is present for axis control with 1500 CPU, but there isn't one for 1200 PLC series. In pdf attached you'll find screens of my program and settings. AttachmentStepper Control.pdf (635 Downloads) |
Last edited by: milos23 at: 08/12/2024 07:30:43 |
|
Follow us on