(0)| 10/11/2024 8:37 PM | |
|
Joined: 1/19/2022 Last visit: 9/23/2025 Posts: 5 Rating:
|
Hello all, I'm currently working on a steam project where we're using a Siemens P320 differential pressure transmitter. We've installed the DP transmitter to measure up to a maximum of 1 bar for our process. However, when we follow the calibration procedure as outlined in the Siemens manual, the transmitter won't go to zero and stays fixed at 2 bar, even after opening the drain valves. I need to know how to get sure if the sensor is damaged or we just missing somthing form SIEMENS ? Has anyone encountered a similar issue or have suggestions on how to resolve this? https://support.industry.siemens.com/cs/de/de/view/109758474/112785759371 |
Last edited by: Moderator_Lan at: 10/14/2024 09:08:31link optimized |
|
Follow us on