10/15/2024 8:55 AM | |
Joined: 9/12/2024 Last visit: 8/27/2025 Posts: 2 Rating:
|
I also have the same problem with a TL-WN725N tp-link WIFI dongle not detected. FS05 In the Siemens documentation iot2050_operating_instructions_en-US.pdf there is a section on "Use USB Wifi dongle to connect the iot2050 to a wireless access point", is this option only available with the Advanced device? If this option is available for the Basic iot2050 device, can you please suggest a suitable usb wifi dongle and instructions on how this should be configured. ------------------------------------------------------------------------------------------ |
Last edited by: Moderator_Lan at: 10/15/2024 09:26:12New subject after splitting |
|
10/17/2024 7:02 AM | |
Joined: 3/12/2024 Last visit: 9/19/2025 Posts: 187 Rating:
|
Hello alastair_long172, I'm sorry to hear that you're having problems with the TL-WN725N WiFi dongle on the SIMATIC IOT2050. Here's some information and suggestions regarding your query:
To get started with your WiFi Adapter follow these steps:
|
This contribution was helpful to
1 thankful Users |
Follow us on