(0)| 11/9/2024 10:48 AM | |
|
Joined: 10/10/2024 Last visit: 5/15/2025 Posts: 3 Rating:
|
hello all, In my project i used plc S7-1200 1214C DC/DC/DC plc AND servo v90pn, Simotics S-1FL6 ABS.MT.20:BIT MOTOR And Drive, I used these in Absolute Rotary Table application, Gear box 50:1 used, so load movement per motor revolution is 7.2 degree, i used modulo(modulo length 360 and start modulo 0.0) for zero degree after completing one revolution of rotary table, and used home mode_7 for one time offset homming, now PROBLEM IS WHEN I ROTATE ONE REVOLUTION OF ROTARY TABLE(50 REVOLUTION MOTOR) USING MOVE_ABS TO 0* COMMAND, MOTOR ROTATE ONE REVOLUTION PLUS SOME EXTRA DEGREE but ACTUAL POSITION SHOWING ZERO. showing wrong degree ,actual table degree is 1 and showing 0, ANY IDEA FOR THIS.?? ------------------------------------------------------------------------------------------ |
Last edited by: chiragvala10 at: 11/09/2024 10:58:18Last edited by: chiragvala10 at: 11/09/2024 11:49:16Last edited by: Moderator_Lan at: 11/11/2024 07:53:41New subject after splitting |
|
Follow us on