(0)| 11/28/2024 3:49 AM | |
|
Joined: 3/10/2022 Last visit: 11/3/2025 Posts: 11 Rating:
|
I have a PCS7 system consisting of ES and two OS Single Stations. The AS is (6ES7656-6CL33-3BF0) SIMATIC PCS 7 CPU410 Redundant consisting of 2xCPU410-5H and 2xCP443-1. I have a CP1623 (6GK1162-3AA00). I am facing difficulty in connecting to WinCC using the CP1623. Now I am trying to put the CP1623 on the Engineering station. I have tried it using the PG/PC to PC internal local1 and also on CP1623 OSO but it doesn’t work. When I download from Netpro I get: The connection to the target module cannot be established. I have tried both s7-connection and s7-connection-fault-tolerant but still not working. I am not sure what the actual problem is, could you please check the attached images showing all the current settings I have in the system. I really appreciate your help in the matter. Thanks AttachmentCP1623ConnectionToWinCCProblem.zip (187 Downloads) |
Follow us on