(0)| 12/3/2024 1:30 PM | |
|
Joined: 3/15/2022 Last visit: 8/4/2025 Posts: 3 Rating:
|
CNet is installed on a PCS7 V9.0 Sp1 Engineering Station using SIVaaS V3.3 on Windows Server 2016. CNet: CNET-03.01.00.00_00.00.09.04-windows-x64 Firmware: cn4100-amd64_factory-03.01.00.00_00.00.00.21 We created and developed a CNet project on our development system which for all intent and purpose is a mirror image of our production system. Since installing CNet on our production system and restoring the archive from our development system we can no longer "Activate" the CN4100 CPU. We get the errors in the attachments. From the engineering station we can ping the CN4100 interface and the NTP Time Server. The only thing we have had to change between the Development environment to the Production environment is the NTP time server IP, everything else is identical. Any help would be greatly appreciated.
Attachmentcnet_errors.zip (135 Downloads) |
Follow us on