12/11/2024 10:29 AM | |
Joined: 3/14/2008 Last visit: 9/11/2025 Posts: 2216 Rating:
|
Hi, Maybe one of the following posts can help you: Do you use a released operating system? Can you create a new WinCC project and does that work? Have you checked access rights for the project folder as described in Compendium part F, page 115 see: Link If you configured a domain from workgroup or vice versa, then have you run the security controller settings again? See page 78 of Compendium part F |
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to
1 thankful Users |
1/5/2025 6:19 PM | |
Joined: 10/5/2016 Last visit: 8/10/2025 Posts: 109 Rating:
|
After deleting and creating a Wincc Client project , we were able to open the project from the EWS |
Follow us on