(0)| 1/10/2025 4:17 AM | |
|
Joined: 1/10/2025 Last visit: 9/4/2025 Posts: 3 Rating:
|
Hi everyone, I have the same issue, i am using cognex camera IS7200 communication with S7-1200 via Profinet. I need suppourt for this issue. Who are there fix it yet? ------------------------------------------------------------------------------------------ |
Last edited by: Moderator_Lan at: 01/12/2025 21:44:40New subject after splitting |
|
| 1/12/2025 5:11 AM | |
|
Joined: 1/10/2025 Last visit: 9/4/2025 Posts: 3 Rating:
|
Hi sir, I have the same issue MrRunning I was config connection between PLC and Camera okay, and then i was test all function, it work fine. But when i turn off power supply and wait some minutes i turn on power supply, the red light on PLC is flash. After that, i open tia portal i see error profinet connection. The camera have an error at function "User Data", then i go to log status of PLC the error logged is as follows: "Error: Cyclic and Asynchronous writes to User Data are being performed. Please choose only one method on Input/Output channel 1 Insight/UserData - 64 bytes." At that time, the PLC can still read status "Online/Offline", "Result 64 bytes" of Camera, only function "User Data" not work. Do you have any method for solve this issue?
AttachmentIssue.pdf (223 Downloads) |
Last edited by: nguyen_hai172 at: 01/12/2025 05:18:56 |
|
| 1/15/2025 2:38 AM | |
|
Joined: 1/10/2025 Last visit: 9/4/2025 Posts: 3 Rating:
|
Hello, I was created new project (don't have code in program, only config communication). This issue still happen. |
Follow us on