(0)| 1/20/2025 8:35 PM | |
|
Joined: 1/19/2025 Last visit: 12/15/2025 Posts: 1 Rating:
|
Hello new to siemens. I'm using TIA v18. i installed GSDML-V2.45-Siemens-ET200SP-20241104.xml.zip (1,6 MB) because it says that is the add on i needed to be able to add 6ES7155-6AU01-0CN0 ET 200SP, IM155-6PN/2 HF to my current program. the file installed successfully but the module is still not showing up under the hardware configuration. anyone run into this? Am I not installing the right thing to have this module show up? I even installed the HSP that said it had it in there and it didn't. Please help. |
| 1/21/2025 3:20 AM | |
|
Joined: 5/12/2006 Last visit: 12/19/2025 Posts: 22816 Rating:
|
check the correct folder in hwconfig the gsd is located under additional field devices |
Follow us on