(0)| 1/21/2025 1:24 PM | |
|
Joined: 10/10/2005 Last visit: 1/29/2025 Posts: 1940 Rating:
|
Hello Emilio Check the installation on your computer to see whether you still have option packages that you need to upgrade after installing STEP 7 V5.7 SP2 Hf1. The behavior you describe indicates an incompatibility. The FAQ also provides help: Check the STEP 7 V5.x project for required option packages You can also use the Compatool to check your installation. If necessary, you will then have to upgrade the corresponding option package. http://www.siemens.com/compatool Another workaround is to make a copy of your project using the menu command "Save as" with the option "With reorganization (slow)". Then continue working with the copy. With best regards |
Follow us on