(0)| 2/17/2025 11:09 AM | |
|
Joined: 3/14/2008 Last visit: 12/28/2025 Posts: 2233 Rating:
|
Hi, The reboot popup is shown when the WinCC application detects a problem with one of the running processes. This could result from other problems with the PC station. It is normal that the station is rebooted when pressing the button. What I always check first is the WinCC diagnose directory under C:\Program Files (x86)\Siemens\WinCC\diagnose. Sort the files by date/time and check which one is last written during the reboot popup. The file: WinCC_Sys_xx.log or SIMATIC_S7_Protocol_Suite_xx.log can give you more info about the error. For example, if a problem is detected with the network card, it could result in the reboot popup or a problem with the WinCC archive manager. If you cannot find anything, you can create a support request and you are asked to upload the files from the diagnose folder and run a program to collect information from the system. |
|
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on