4/24/2019 3:07 PM | |
Posts: 4 Rating:
|
I have problem in installation s7-PLCSIM V13 , in the end of installation writ '' An error occurred during setup , and show that system has not modify ,,,in installation log show BUNDLE: S7-PLCSIM V13.0 SEBU Version: PLCSIM_V13:13.00.00.00_02.04.00.01 OS: Microsoft Windows 7 Home Premium Home Premium Edition, Service Pack 1, 64-bit, build 7601 COMMANDLINE: C:\Program Files (x86)\Common Files\Siemens\Automation\Siemens Installer Assistant\305\SIA2.exe /starter /bundlepath=C:\USERS\SEBIAT\DOCUMENTS\PROGRAM\TIA PORTAL V13\SIMATIC STEP7 V13 PLCSIM\SIMATIC_S7_PLCSIM_V13\InstData INSTALLDIR: C:\Program Files (x86)\Siemens\Automation SETUPLANGUAGE: 1033 CHANGES: (+)DotNet_Updater;(+)S7_PLCSIM_TIAP_V13;(+)PlcSimPlus64;(+)PlcSimPlus There are NO severe messages before the installation 12:41:39 | BEGIN. Execution started. 12:41:50 | OK RunningProcesses (), Complete 12:41:53 | OK InventoryBefore (A), Complete 12:41:54 | OK Citamis (Before), Complete 12:41:54 | OK StartApplBefore ([INSTALLDIR]BIN\SIEMENS.AUTOMATION.OBJECTFRAME.FILESTORAGE.SERVER.EXE), Complete 12:41:55 | OK StartApplBefore ([INSTALLDIR]X64\BIN\SIEMENS.AUTOMATION.OBJECTFRAME.FILESTORAGE.SERVER.EXE), Complete 12:41:55 | OK ClassicCompPrepare (), Complete 12:41:55 | OK ProductRegistration (Before), Complete 12:41:55 | OK ClassicCompAfterUninstall (), Complete 12:41:56 | OK SetupUnit (DotNet_Updater), Complete - - Foreign, AddLocal 12:41:57 | OK SecurityControl (S7_PLCSIM_TIAP_V13), Complete;Before 12:43:20 | OK SetupUnit (S7_PLCSIM_TIAP_V13), Complete - - PlusMain, AddLocal 12:43:22 | OK SecurityControl (S7_PLCSIM_TIAP_V13), Complete;After 12:46:35 |ERROR AdsWorkerClassicComponent::OnWorkerCompleted(): - ClassicComponent setup result: Failed: Value = -11 (TIMEOUT) 12:46:35 | FAIL! SetupUnit (PlcSimPlus64), Failed - - ClassicComponent, AddLocal 12:53:17 | OK RebootAfterAll SetupUnit (PlcSimPlus), Complete - - PlusOptional, AddLocal 12:53:18 | OK ClassicCompAfterInstall (), Complete 12:53:18 | OK ClassicCompRollback (), Complete 12:53:19 | OK HspInstall (), Complete 12:53:19 | OK StartApplAfter ([INSTALLDIR]BIN\INSTALLROOTCERTIFICATE.EXE), Complete 12:53:40 | OK StartApplAfter ([INSTALLDIR]BIN\SIEMENS.AUTOMATION.GENERATOR.FRAMEWORK.EXE), Complete 12:53:41 | OK StartApplAfter (C:\WINDOWS\SYSWOW64\S7EPATSX.EXE), Complete 12:53:42 | OK StartApplAfter (C:\WINDOWS\SYSWOW64\S7EPAESX.EXE), Complete 12:53:44 | OK ProductRegistration (After), Complete 12:53:48 | OK SetupIsComplete (), Complete 12:53:51 | OK InventoryAfter (Z), Complete 12:53:52 | OK LicenseTransfer (), BeforeStart 12:53:52 | OK Citamis (After), Complete 12:53:52 | OK SetupSummary (), Complete 12:55:13 | OK SetupReport (), Complete 12:55:13 | END. Execution completed. Exit code: 1603 Errors: 1 Warnings: 0 Exit code means: Installation failed (InstallFailure) What i have to do ???? ------------------------------------------------------------------------------------------ |
Last edited by: boumsoum at: 04/24/2019 15:09:42Last edited by: boumsoum at: 04/24/2019 15:11:13Last edited by: boumsoum at: 04/24/2019 15:24:00Last edited by: Jen_Moderator at: 04/25/2019 10:27:14New subject after splitting |
|
4/24/2019 3:09 PM | |
Joined: 5/12/2006 Last visit: 9/2/2025 Posts: 22709 Rating:
|
Hello, can you post the complete Logfile, not only a line? Christoph |
4/24/2019 3:17 PM | |
Posts: 4 Rating:
|
hello ,, yes this is complet logfil |
6/1/2025 1:41 PM |
|
Joined: 6/1/2025 Last visit: 6/1/2025 Posts: 1 Rating:
|
You ask for something without giving information from where and what he should post more. Useless |
Follow us on