8/20/2025 9:44 AM | |
Joined: 8/3/2009 Last visit: 9/12/2025 Posts: 16409 Rating:
|
Hello mohammad_siami83 It should work to communicate with PLC Sim Advanced over ethernet to external communicatin partners (now thats one of the main reasons for PLC Cim Advanced). OPC UA Server should also work in this simulation but only without security. Here is a FAQ how to connect PLc Sim Advanced to (also real) Siemens HMIs . perhaps the steps are quite similar to your situation: https://support.industry.siemens.com/cs/de/en/view/109748099 I have also used PLC Sim Advanced already for communication with external systems so basically it should work. Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on