(0)| 10/8/2009 9:16 AM | |
|
Posts: 9 Rating:
|
Dear All, I am using Siemens make Micro Master 440 (7.5KW) for Puller Drive application. Puller Drive will pull the Aluminum duct from Aluminum extrusion Machine. Here I want to control the Puller drive speed based upon the Aluminum extrusion machine speed with torque. I done all the SLVC Parameter settings. Now Aluminum machine speed increase means Puller drive speed increase automatically and Aluminum machine speed decrease means Puller drive speed decrease automatically with quick response but torque was not controlling in this mode. Here I want to control the Puller Drive Torque also. If machine speed increase then puller drive torque also should reduce and machine speed increase then puller drive torque should increase. How can I solve this problem? Iattached the Application details and Parameter detailsfor your kind reference. Kindly give your valuable suggestions to me. Advance in thanks AttachmentApplication_1.pdf (362 Downloads) |
Last edited by: O_Moderator at: 10/8/2009 10:27 AMquestion transferred from another thread |
|
| 10/24/2009 7:34 AM | |
|
Posts: 17 Rating:
|
dear muthu... read P1960... This can also help you.. |
Follow us on