(0)| 12/4/2009 1:52 PM | |
|
Joined: 9/27/2006 Last visit: 1/12/2026 Posts: 12480 Rating:
|
Hello Vinay; Which model of IM do you have in your S5 configuration, which type ofnetwork? In S7 hardware, IMs are used exclusively for extension racks. Network communications use CP modules, and these can use many cards in parallel without problem. So a description of your setup would help us clarify your requirements. A sketch of your present S5 configuration would be most helpful. Hope this helps, Daniel Chartier Edit: Just today Howard Wong posted an application note showing the conversion of various S5 modules to S7 conterparts. Look at hios post in the following link, and check out what the S5 IMs can be converted to in an S7 environment: /tf/WW/en/Posts/37834#top D.C. |
Last edited by: dchartier at: 12/4/2009 2:38 PM |
|
Follow us on