(0)| 4/8/2010 11:43 PM | |
|
Posts: 223 Rating:
|
How can you set the system time of Simotion from within the code (like you can set the time in a S7 PLC with SFC 0 1). |
| 4/9/2010 7:48 AM | |
|
Posts: 116 Rating:
|
Hi, see function manual "SIMOTION Basic functions" (Release 5/2009: page 415) --> Real-time clock RTC http://support.automation.siemens.com/WW/view/en/27002431 Synchronize time to SINAMICS If you want to synchronize the TIME to SINAMICS or SINAMICS Integrated of SIMOTION D, there is a nice sample: --> seeSIMOTION Utilities & Applications (SIMOTION Utilities & Applications is part of the delivery of SIMOTION SCOUT).
|
Last edited by: Jerry at: 4/9/2010 8:01 AM |
|
| 4/12/2010 11:27 PM | |
|
Posts: 116 Rating:
|
Hi, see: http://support.automation.siemens.com/WW/view/en/26234196 Time synchronization between HMI master (e.g. WinCC), SIMOTION and HMI slave (e.g. WinCC flexible) Have also a look to the SIMOTION Utilities & Applications ---- there you'll find lots of FAQs and sample programs. You find SIMOTION Utilities & Applicationson one of the SCOUT DVDs. Regards Jerry |
Follow us on