(1)| 9/19/2010 9:47 AM | |
|
Joined: 2/10/2010 Last visit: 4/16/2025 Posts: 35 Rating:
|
Dear all. I have a problem with technology blocks FB 401 MC_Power and FB 414 MC_MoveVelocity startup in my program for SIMODRIVE 611U. The structure of my project is: FB100 FB 401 MC_Power (to enable or disable an axis.) FB 402 MC_Reset (to acknowledge all errors accepting acknowledgment in the user program) FB 405 MC_Halt (stops all motions and brings the axis to a standstill. The standstill position is not defined) FB 414 MC_MoveVelocity (initiates acceleration of the axis to the preset velocity)
Mode 0 – Speed-controlled axis: Speed-controlled (speed-controlled axis without encoder) MC_MoveVelocity" PositionControl = FALSE Mode 4 – Simulation mode. The purpose of the program simulation mode is to test the programmed sequences in the controller, as well as the interaction between different axes. The axis is not moved during this testing! Block FB 414 MC_MoveVelocity gave out parameter of error ErrorID 8044 at activation I0.3 (Command not supported by the technology object. For example, using the "MC_Power" at an output cam.) Axes are configured manually [2]. There are true parameters on inputs of all FB blocks are set, according to a manual [1]. 3.SIMATIC S7-300 Connecting the SIMODRIVE 611U to the Technology CPU 5. Similar problem: /tf/WW/en/Posts/37283 AttachmentScreenshoots.zip (350 Downloads) |
| 9/19/2010 1:00 PM | |
|
Joined: 7/28/2010 Last visit: 8/31/2024 Posts: 184 Rating:
|
Max, Make sure your Axis Number is correct. Axis number is the number of DB which is assigned to your Axis by using Technology Objects Management (TDM). You have set the axis number to 2, you should have a DB2 which has all the data for that axis in it. Regards, Behnam www.sigmaprocess.ca |
This contribution was helpful to
|
|
| 9/22/2010 11:37 AM | |
|
Joined: 2/10/2010 Last visit: 4/16/2025 Posts: 35 Rating:
|
It works! Thank you for good thoughts |
Follow us on