(0)| 2/5/2012 6:52 AM | |
|
Joined: 3/21/2006 Last visit: 10/16/2025 Posts: 10239 Rating:
|
Hello, Yes, there have possibility to reach drive viq S7-300 rounting. Check if you trype of CPU supports routing. What are the requirements for using the S7 routing function and which modules can you implement? Then you must configure a Netpro connection.Routing among PROFIBUS subnets on one CPU 400 using the DriveMonitor of DriveES Best regards, Hristo Mihalev |
| 2/5/2012 9:56 PM | |
|
Joined: 10/7/2005 Last visit: 12/29/2025 Posts: 3052 Rating:
|
Hello riss even thoughproperrouting setup is a must have for routing to work as mentioned by UMENCHO, I fearit is NOT going tohelpyou in this case and ampretty sure that a 6RA24 does generally NOT support online programming access via Profibus (neither with a CB24 not with theolder CS51 board). Below is aFAQ thatat least confirms that Drive Monitor can not be used via Profibus on a 6RA24/CB24 combination: How can I use DriveMonitor in conjunction with the 6RA24? Most likely not the answer you wanted to hear, but I hope it helps anyhow and perhaps one of our Drives Experts here can confirmthis (if not, send a Service & support request to Siemens and let us know their answer) P.S.: It is definetely possible with the 6RA70 (successor to the 6RA24) and of course the Sinamics 6RA80 (latest generation of the Siemens DC Drives). |
Last edited by: fritz at: 2/6/2012 4:46 AMmore typos fixed Last edited by: fritz at: 2/5/2012 10:00 PMtypos Cheers |
|
Follow us on