1/6/2012 4:23 PM | |
Posts: 46 Rating:
|
I have a redundant system of two CPUs 6ES7 417-4HL00-0AB0. Current condition of the CPUs are: RACK_0 CPU:EXTF(Lit), BUS2F(Blink_Blinking rate almost 2Hz), RUN(Lit), REDF(Lit), IFM1F(Lit), IFM2F(Lit), MSTR(Lit), RACK0(Lit) RACK_1 CPU: All Leds are Flashing I also have a fault in a DP called DP 11. I attached the pictures of the DP in the Attachement. In that particuler IM module SF(Lit) and BF(Flashing). I couldn't go online with RACK_1 CPU. I abled to go online with the RACK_0 CPU. Attached is the screenshot of the Hardware Configuration with Diagonostic Buffer of the RACK_0 CPU which is now taking care the system. Please guide me to recover from this condition. --- Thanks AttachmentAttachment_1.zip (446 Downloads) |
Follow us on