(1)| 4/6/2012 8:36 PM | |
|
Joined: 7/8/2009 Last visit: 6/7/2025 Posts: 1977 Rating:
|
Well then, you must not use SLVC Have a look at following FAQ http://support.automation.siemens.com/WW/view/en/14390055 Now try making some more smaller ramp time say 0.5-0.8 Sec And what I feel is, itshould befaster enough. Because I assume your motor is 4Pole, then Rated speed will be 1500. In this case you want to run at 200RPM which is at 6.7Hz so for 1sec Ramp up time, it will take 0.13 sec to reach your desired setpoint Now I think thats faster enough but still you can try setting ramp up still smaller And what is Magnetisation time you have set? You can reduce a bit but dont make it much lower Contactor Logic can give instant start-stop but at that time you will get full speed so crane will move with a Jerk and may be due to speed differnce also you may not able to compare clearly Regards Devesh Vithani |
|
I dont Like people driving Fast, thats the reason I overtake them ;) |
|
Follow us on