(0)| 3/28/2007 11:06 AM | |
|
Posts: 262 Rating:
|
Hi fishDMX, for your cpu current please use the rated current only. Pleasee note that cpu31x consume current from external 24V supply while cpu41x consume internal 5V supply. For periferals please note that these are consuming current from an internal supply provided by the cpu (backplane) and also from the external 24V supply (L+). The internal 5V supply provides up to 1A. Good luck |
| 3/28/2007 5:23 PM | |
|
Posts: 3 Rating:
|
Thanks for the answer. A lost question about the periferals. For instance, a periferal module consumes 0,1A of the backplane (5V). How much do I have to take in the count of this 0,1A (5V) for my power supply (24V). Or is the maximum backplane current consumption already integrated in the rated current of the CPU? |
| 3/29/2007 9:59 AM | |
|
Posts: 262 Rating:
|
Hi fishDMX, the current consumed from backplane is included in the (max) rated cpu current, so you don't calculate the backplane current to 24V circuits. Good luck |
Follow us on