(0)| 8/19/2013 11:16 AM | |
|
Posts: 262 Rating:
|
Hi, As I can understand you have "Profinet module" having MLFB 7KM93-0AE00-0AA0. If you have profinet module then you can connect 50devices in a ring can use PN port of S-7 300 CPU directly to read its data. The above module is phased-out and replace with a new one... however, one more suggestion, please refer the below link and upgarde the firmware of this module. https://support.automation.siemens.com/WW/llisapi.dll?func=cslib.csinfo&lang=en&objid=7KM9300-0AE00-0AA0&caller=view To upgarde firmware you may require to install Power Config software which can be searched inthis site only or refer below link https://support.automation.siemens.com/WW/llisapi.dll?query=powerconfig&func=cslib.cssearch&content=adsearch%2Fadsearch.aspx&lang=en&siteid=csius&objaction=cssearch&searchinprim=0&nodeid0=25240973&x=8&y=5 |
| 5/21/2014 9:21 AM | |
|
Posts: 340 Rating:
|
new question is splittet to communicate cpu-315 2pn/dp with an instrument (electronite multilab-3) over ethernet. |
Follow us on