(0)| 7/29/2014 6:16 PM | |
|
Posts: 5225 Rating:
|
Hi there. From a user standpoint - I would not be too happy to grab a PC to make some timer changes. There is the option to use the built-in screen on the LOGO! to create user pages for making adjustments available. I use that regularly. With the LOGO! inside the cabinet you also ensure only some have access to it. BUT you will have to make sure of the safety factors so that someone does not cause harm to himself while doing such changes. Alternatively would this suit you?.. {link} ![]() Greetings. w |
| 7/29/2014 10:06 PM | |
|
Posts: 5225 Rating:
|
Hi-ya, You are the "king" of your own project.. you can decide how you want to run it. I offer my opinion for the alternative. I am the wrong guy to ask about linking LOGO with PC with a user designed PC program. But design custom communication programs may as well cost you more in the long run. At least with the hardware you know what the costs are. It is also more natural to have as a user interface. That is my experienced opinion. But then again your client may be less rough-and-tough than my clients. [smile] The text display gets its messages from the LOGO.. also you use the same mechanism to put messages on the built-in display of the LOGO. Please look at the [LINK]. Come back and tell us if the text display is not an option. I am sure there will be someone here that will be able to help you out. Greetings. w |
| 7/30/2014 8:36 AM | |
|
Joined: 4/22/2010 Last visit: 3/31/2025 Posts: 5697 Rating:
|
Hello, I suggest you have a look at the Logo! application examples, in the Section Display you will find the Menu Control example, study this example and you will learn how to use the Display and how to change values, if you use the Logo display only, you will have no function keys, use the cursor keys instead. By the way if you use the searchfield in the upper right corner i'm sure you find plenty examples of what you planned to do. Here is one to start with. Setting timer value from Keysregards, Marcjan |
Last edited by: Marcjan at: 7/30/2014 9:04 AMProblem solved? |
|
This contribution was helpful to
|
|
| 7/30/2014 4:18 PM | |
|
Posts: 9 Rating:
|
First of all, thanks people! And yes, I guess that using a PC is kind of overrated for this simple hour control. But I was asked to see if there was any way to implement it. Also I´m using the cursor keys already. Thanks once again. C. |
Follow us on