(0)| 7/1/2015 1:04 PM | |
|
Posts: 45 Rating:
|
hi! I can not view the 0BA8 logo menu in the web server. or handle it from seveur seveur displays the elements of the logo (see attached file) and I can do anything please help me with a practical example Attachmentfichier.docx (255 Downloads) |
| 7/1/2015 2:27 PM | |
|
Joined: 12/18/2014 Last visit: 12/28/2025 Posts: 36382 Rating:
|
In this Topic: i wrote to you, that the webserver only can show you message texts, no menus of the logo. |
| 7/1/2015 2:36 PM | |
|
Joined: 12/18/2014 Last visit: 12/28/2025 Posts: 36382 Rating:
|
For example see attachment.
Attachmenttest.zip (213 Downloads) |
This contribution was helpful to
|
|
| 7/1/2015 5:27 PM | |
|
Joined: 12/18/2014 Last visit: 12/28/2025 Posts: 36382 Rating:
|
Can you even describe precisely what you want to do? |
This contribution was helpful to
|
|
| 7/1/2015 5:52 PM | |
|
Posts: 45 Rating:
|
I realized this little test on the training bench 0BA8 logo (see attached file) inputs I1, I2, I3 and I4 are connected to sensors; the outputs Q1 and Q2 lamps the system works well when different sensors are activated physically I want to control the system from the web server how to do? AttachmentProject.rar (250 Downloads) |
| 7/1/2015 6:13 PM | |
|
Joined: 12/18/2014 Last visit: 12/28/2025 Posts: 36382 Rating:
|
From the Web server, you can not directly inputs or outputs switch (forcing). Outputs would only be possible if you are not driven in the program (by variables). If you want to make the Web server by, you must use the virtual keys on the logo and / or the TDE. You would need to program a message texts via menu and link the buttons accordingly. A boarding aid in attachment. It is not complete, but it is enough for a glimpse.. Attachmentcomfortable_menu_navigation.zip (255 Downloads) |
This contribution was helpful to
|
|
Follow us on