(0)| 12/12/2007 5:01 PM | |
|
Posts: 739 Rating:
|
Hi Soma, did you set up the Parameter of the drive well? If not please follow the instructions. http://support.automation.siemens.com/WW/view/en/21694875 If you seted up well, I need to have more details. |
| 12/13/2007 10:45 PM | |
|
Posts: 112 Rating:
|
What is the frequency on the motor name plate? |
| 12/14/2007 8:28 AM | |
|
Posts: 739 Rating:
|
Hallo John, your problem can be electrically as well as mechanically. Mechanical it can be a bearing of the motor or pump. Electrall it can be a defect in the motor, in the cable or in the drive. But it is also possible that it might come from the medium witch you have to pump (or a change in the pipe system). I suggest that you collect all available information (e.g. technical data of the drive, the motor, and the pump) and that you contact the technical support they are able to help you. ------ |
| 12/14/2007 3:42 PM | |
|
Posts: 4 Rating:
|
50 HZ |
Follow us on