(0)| 1/15/2008 1:01 AM | |
|
Posts: 130 Rating:
|
The reason i said check the connector is a poorly connected sheild can cause wierd problems on profibus. Also, i have had connectors where the leads broke, but made intermittent contact. Its an easy one to check anyway. You should be able to use up to 31 devices w/o a repeater. The last project i used a repeater anyway (30 devices) anticipating i would need it for troubleshooting. It seems a bit odd to me that your errors are limited to specific hardware. Perhaps you could try swaping the profibus card with another. The system i integrated with 18 MM420's had one bad profibus adapter. I had similiar problems but just with that specific module. Perhaps this thread helps /tf/WW/en/Posts/9444 |
Follow us on