(0)| 5/12/2015 1:12 PM | |
|
Posts: 16 Rating:
|
Need help to find feasibility. Application: GPS (CMR2020 with GPS Antenna) Mounting in train, as train reaches to defined location activate relay output. Query: 1. Is it possible to use only GPS antenna to find out GPS location, or GPRS antenna also required to assist?( I mean Is GPRS antenna mandatory?) 2. Can CMR 2020 module give location co-ordinates to LOGO PLC in some register, to compare it with defined Co-ordinates? If yes Which register and how to access? 3. If you have such example available with logic or settings please forward. Thank you.
---------------------------------------------------------------------------------------------------- |
Last edited by: Min_Moderator at: 5/12/2015 3:47:46 PMNew subject after splitting |
|
| 9/10/2015 12:00 PM | |
|
Posts: 2930 Rating:
|
Hi, here an example how to get the GPS information from a CMR to LOGO! VM-Memeory. During the CMR configuration you can select the start adress of the GPS infomration. Here VB100. If you need it for Datalog just take the info you need out of the LOGO! VM-Memory by using a NAI to a analog amplifie --> open connection.
AttachmentGPS trac astro.zip (260 Downloads) |
Follow us on