(0)| 10/21/2015 3:54 PM | |
|
Posts: 1 Rating:
|
We are facing some problem to control the speed of VFD 440 from the BOP. Now it is not possible to change the speed from BOP with the present program. Could you please anybody advice me the correct program and [please see below for the program we set. P0003 -3 P0010 -0 P0700 - 0 P0701 -16 P0702 -1 P0731 -52.2 P0732 - 52.3 P0756 -2 P0757- 4 P0758-0 P0759-20 P0760-100 P0761-4 P1000-23 P1001-50 P1002-0 Our Analog input and output is 4-20mA and our control as we need to control the VFD through BOP during manual and through analg input during Auto selection. But now as per the existing program we cant able to control through BOP. ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 10/21/2015 4:06:27 PMNew subject after splitting |
|
Follow us on