(0)| 2/19/2008 4:44 PM | |
|
Posts: 151 Rating:
|
The basic structure of the firmware in AFE and CUVC / CUMC ist different. It is like for older CU1 / CU2 / CU3. So in the chap.8.2 of the compendium anything said regarding CU1 / CU2 / CU3 states for AFE, too. Acyclical communication is possible to CBP2 with DS100.DS47is possible, if the firmware of CBP2 is V2.23. Acyclical communication to older CB1 is NOT possible. You can read out the parameters, observing the chap. 8.2.3 of the compendium. For example r947 / 949 / 953 to 960 http://support.automation.siemens.com/WW/view/en/23660019 |
Follow us on