(2)| 4/11/2016 9:38 AM | |
|
Posts: 8092 Rating:
|
Please provide the detail MLFB number of MM440 & the motor connected to it. |
This contribution was helpful to
|
|
| 4/11/2016 10:58 AM | |
|
Posts: 16 Rating:
|
MM440: 6SE6440-2AD24-0BA1 Motor: ABB motor / 0.37 kW / 380V / 1.4A / 0.78 cos f / 810 rpm |
| 4/11/2016 11:30 AM | |
|
Posts: 203 Rating:
|
Hello, Normally in this type of applications a mechanical brake is used to hold the load and prevent reverse rotation during stop and during power off |
Follow us on