(0)| 6/5/2016 5:08 AM | |
|
Posts: 1 Rating:
|
Hello I have simatic step 7 version 5.5 and drive monitor installed 5.5. I received PLC software project and it cames with Simoreg DC master, but when I retrieve this project I am not able to see these two Simoreg DC. Do you guys have any ideia why is it like that ? ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 6/6/2016 10:32:20 AMNew subject after splitting |
|
| 6/5/2016 5:25 AM | |
|
Posts: 8092 Rating:
|
In your Simatic Step 7 V 5.5 hardware catalog please check if Simoreg DC master is available. If not you need to install Simoreg DC master GSD files in step 7 hardware catalog. Simoreg DC master GSD files are available at below link. GSD- and EDS-File for 6RA70 SIMOREG DC-MASTERHTH. Or please check the DC drive release version & Step 7 DC master drive version compatibility. |
Last edited by: PISCEAN 2010 at: 6/5/2016 6:11:40 AMLast edited by: PISCEAN 2010 at: 6/5/2016 12:41:29 PM |
|
| 6/6/2016 7:49 AM | |
|
Joined: 3/21/2006 Last visit: 10/16/2025 Posts: 10239 Rating:
|
Hello, Like an option is using Drive ES software package... It is apitty why the same has been announced in Product cancellation/discontinuation phase...ok,it is OFT. Best regards, Hristo Mihalev |
Follow us on