(0)| 10/3/2016 8:47 PM | |
|
Posts: 413 Rating:
|
video |
| 10/3/2016 11:03 PM | |
|
Posts: 413 Rating:
|
on the photo wiring diagram ... I need a normal stop (motor shaft free running)... possibly overtorque? |
Last edited by: _oleksandr_ at: 10/3/2016 11:04:25 PM |
|
| 10/5/2016 10:07 AM | |
|
Posts: 8092 Rating:
|
Hello _oleksandr_, Two alternates I would suggest you. 1. Which is the system for control of height adjustment of plasma & oxy fuel torch. Study the same & you can hard wire the interlocks to CNC controller which in turn disables drive. 2. Just install capacitive proximity switch on plasma & oxy fuel head bottom side & adjust the gap between switch & plate material in such a way that it must operate when the torch is about to hit plate material. Hard wire up this contact with CNC controller emergency switch input logic. HTH. |
Follow us on