(0)| 10/24/2016 9:00 PM | |
|
Posts: 3 Rating:
|
What kind of setup i have to build when i have a two 230VAC power feeds (main and backup) and i whant to own power supply to CPU and ext.cards and other power power supply IO field loads. Okay, i have to install "PS" power supply to slot 0 and "PM" power supply to where? DIN rail or can it be left side of "PS" power supply? Other way is to install two "PM" power sypply's and one is feeding system power and second is feeding field load. Correct? Thanks. ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 10/25/2016 4:29:24 PMNew subject after splitting |
|
Follow us on