(0)| 2/23/2017 8:56 AM | |
|
Posts: 3 Rating:
|
Hi! I'm controling a elevator with a G120c. and i am having trouble when i am loading the lift with about 500 kg. And this is the first time i am using starte,. so i dont really know what parameters to use. i was first using [1] standard drive control. and was able to drive the lift up. but the DC braking was not working on the way down. and the drive sroped due to overspeed. i then tried [2] dynamic drive control so i could change the parameter 1400-1498 but without success. i can drive the lift with about 200 kg in [2] dynamic mode without any problems. but when i use 500 kg i cant even drive it up. if anyone knows what parameters to use i would be really gratefull Attaching some screed dumps of my parameters. Attachmentstarter_param.zip (309 Downloads) |
| 2/23/2017 9:51 AM | |
|
Posts: 531 Rating:
|
Is the brake really big enough for slowing the drive down or only for securing at stand still? |
| 2/23/2017 10:47 AM | |
|
Posts: 3 Rating:
|
i solved it now. i did not see p219. so the brake power was on 0kW.... now it is working great |
Follow us on