(0)| 8/3/2017 11:19 AM | |
|
Joined: 4/28/2015 Last visit: 4/24/2025 Posts: 3345 Rating:
|
Hi, you can have a look here. Maybe it has something to do with the termination? Best regards! |
|
Not working for IOT2050 support anymore from March 1st, 2024. |
|
| 8/4/2017 8:52 AM | |
|
Posts: 48 Rating:
|
Can you provide a connection diagram from MAX485 to the IOT2020 ? Important is the connection and timing of the send/receive pin of MAX485 (RE/DE). |
| 8/4/2017 9:48 AM | |
|
Joined: 1/26/2012 Last visit: 4/6/2025 Posts: 102 Rating:
|
Ciao Ocean_ I think that the problem is RE/!DE. It driving me nuts! I use this code for sending and receive the data:
see the attached files for a diagram. When I send the data from IOT, the trasmission is always good but the receive data some time is no good e sometime is ok. If I stay in listen and send a data with the monitor device, the data received from the IOT is always good. Massimiliano AttachmentFoto.zip (231 Downloads) |
Follow us on