(0)| 7/19/2008 4:20 PM | |
|
Posts: 63 Rating:
|
At the begining you have to find on whitch pakckage are based PID controllers in your system. If you have CPU928 (928B) they may use ComregR64 or Modular Fuzzy PID. In other CPU's it's probably the second package. You can made a simple check: 1. If CPU memory cointains large and protected block FB102 (only CPU928/928B) it's probably R64. 2. If there are blocks FB63 (ANLAUF), FB69 (ORGANI) your PID loops are based on Modular PID. Link to support page with documentation |
| 7/24/2008 12:10 PM | |
|
Posts: 150 Rating:
|
dear GrzegorzG thnks for response. My cpu is CPU 948 And blocks Called are FB 245(CNT MODE), FX 202 (REF ADJ), FB 98(RLG: PID, FB 246 (CNT-STAT) All above Blocks are called in pb 179 to pb 227 in same fashion, Now wht should i do if i want to add a new pid controller with the same fashion, I can send u backup of s5 programm if u will need to check. pls help thnks in advance |
| 8/11/2008 4:13 PM | |
|
Posts: 150 Rating:
|
dear edr, there is no such call, pls suggest further how to proceed thnks in advance regards simaticmanager |
Follow us on